1. What can you do with MPS Designer
Welcome to MPS DC/DC Designer Center!
MPS DC/DC Designer is a tool used to create and analyze power supply circuits using MPS regulators. With DC/DC Designer, you can:
- 1) Create and analyze a power supply circuit tailored to your application circuits with a user-friend GUI.
- 2) Choose the MPS regulator best suited for your application from the large number of MPS regulators in the library.
- 3) Choose and tailor the key external component values to optimize for your design such as inductors, capacitors, and compensation values.
- 4) Input target performance specs and let the tool automatically optimize the external component values to meet them.
- 5) Run the circuit and output key performance data such as efficiency, transient performance, and loop stability and view key waveforms such as ripple, switching waveforms, and others.
- 6) Generate a schematic, layout guidelines, and a bill of materials for your design.
2. Main Page Introduction
3. Chip Selection
There are two ways to select a chip:

(1) Select a chip in the database
MPS DC/DC Designer provides a good chip searching function to help you find the chip. Most of the time, you just want to find a chip with the special function and do not want to see the other parts without the function. It can be done by clicking the Search Parts button, and the database for searching will come out like below.

The descriptions for some filter conditions are as below:
1) Part Number: If you enter the part number of the chip here, the expected chip will come out directly.
2) Type: This condition determines whether the chip is the synchronous or not. Sync represents synchronous part, NonSync represents non-synchronous part, and Ignore represents any is ok.
3) Vin(V): The Min&Max filter values determine the chip's minimum and maximum recommended input voltage in the datasheet.
4) Iout Max(A): The Max fliter value determines the chip's maximum recommended output current in the datasheet.
5) Fsw(kHz): The Min&Max fliter values determine the chip's operating switching frequency in the datasheet.
6) Channel: This condition determines whether the chip is single channel or not. Single represents single channel part, Multiple indictaes that the number of channels is greater than 1, and Ignore represents any is ok.
7) Power Good: This condition determines whether the chip has power good pin or not. Yes represents the part has this pin, No represents the part does not has this pin, and Ignore represents any is ok.
8) External SS: This condition determines whether the chip has soft-start pin or not. Yes represents the part has this pin, No represents the part does not has this pin, and Ignore represents any is ok.
(2) Select a chip through the pull-down list
The software also allows you to choose a part through the pull-down list. The only thing need to do is to left-click the pull-down list arrowhead and select a part what you want, and then it is ok. The following figure shows you how to do it.

4. Edit Parameters
When you finish the chip selection, you can edit the circuit parameters to get the simulation result what you want. Different parameters will lead to different power solution result and different electrical performances. So, this job is very important. Fortunately, MPS DC/DC Designer has a set of default parameters which is corresponding to the part. Usually, different chip has different default parameters and these values are according to the EC parameters in the datasheet.
You can edit the parameters according to the following way shows.
4.1 Input Main Specs
The Input Main Specs is about the basic power stage requirement of a design.

The detailed description is as below:
1) Input Voltage (V): The typical input voltage value of the design. The value should be between the minimum and maximum recommended input voltage value which can be found in the chip's datasheet. Otherwise, a warning will occur.
2) Output Voltage (V): The output voltage value of the design. The value should be between the FB voltage and the maximum duty cycle times by input voltage value. The FB voltage and maximum duty cycle can be found in the chip's datasheet. Otherwise, a warning will occur.
3) Output Current (A): The maximum output current value of the design. The value should be between the 0 and the maximum output current value. The maximum output current value can be found in the chip's datasheet. Otherwise, a warning will occur.
4) Switching Frequency (kHz): The operating switching frequency value of the design. If the chip does not have frequency synchronization function, this value will be fixed and can not be edited. If the chip has frequency synchronization function, this value is active. And the value should be between the minimum synchronous frequency and the maximum synchronous frequency value. The minimum synchronous frequency and the maximum synchronous frequency value can be found in the chip's datasheet. Otherwise, a warning will occur.
4.2 Input Optional Specs
The Input Optional Specs is about the special requirement of a design.

The detailed description is as below:
1) Inductor Current Ripple (%): The ratio of the inductor current ripple to the DC amount of the inductor current. If edited by user, the value should be between the recommended minimum and maximum values.
2) Input Voltage UVLO (V): The input voltage threshold of the design. The default value is 80% of input voltage value. If edited by user, the value should be between the InThresholdVoltage and the input voltage value. InThresholdVoltage can be found in the chip's datasheet. Otherwise, a warning will occur.
3) High Current of Transient (A): The high value of the transient output current. The default value is equal to the output current value. If edited by user, the value should be between 0 and the output current value. Otherwise, a warning will occur.
4) Low Current of Transient (A): The low value of the transient output current. The default value is equal to half of the high current of transient value. If edited by user, the value should be between 0 and the high current of transient value. Otherwise, a warning will occur.
5) Slew Rate of Transient (A/μs): The slew rate of the transient output current. The default value is equal to 1 A/μs. If edited by user, the value should be a positive value. Otherwise, a warning will occur.
4.3 R3/C6 Arrangement

The R3/C6 Arrangement determines the type of feedforward compensation. There are two types including A1 and A2.
4.4 Output Cap Type

For some parts, the capacitor type needs to be selected from the Output Cap type drop-down box. There are three types in Output Cap Type drop-down box, including Ceramic, Electrolytic, Ceramic plus Electrolytic.
1) If Ceramic type is selected, it means that user wants to use the ceramic type of capacitor only. This type of capacitor has a standard database in the software. All the ceramic capacitor results come from this database.
2) If Electrolytic type is selected, it means that user wants to use the electrolytic type of capacitor only. You need to input the capacitance value and ESR value manually as there is no database for this type of capacitor.
3) If Ceramic plus Electrolytic type is selected, it means that user wants to use both the ceramic and electrolytic types of capacitors. And ceramic capacitors come from the standard database; while for electrolytic capacitor, user may need to input the capacitance value and ESR value manually.
5. Edit Schematic
MPS DC/DC Designer can give a recommended schematic automatically. You can change it if you are not satisfied with it.
Usually, there are two types of components in a power stage system which includes the main power stage components and the compensation components. Both of these types of components can be changed by user in the software. In order to offer a good analysis function, MPS DC/DC Designer allows user to change the power stage and compensation components separately. If you want to do it, please refer to the following steps.
5.1 Power Stage Components Edit

If you want to change the power stage components manually, the Manually Change Power Stage button which is in the left bottom corner should be selected first. Then, if you hover the cursor around the power stage components, the cursor will turn into a palm symbol which means that the component is allowed to be changed. Left-click the component with the mouse, the corresponding component database will appear.
The power stage components which can be changed are as below.
(1) The Input Capacitor
If you click the input capacitor C1, a capacitor database for searching will come out. Then, you can key the filter value to find the expected capacitor.

The filter conditions include the following items:
1) Part Number: The part number of the capacitor components.
2) Vendor: The vendor of the capacitor components.
3) Material: The material of the capacitor components. The X5R and X7R materials are available.
4) Capacitance (uF): The capacitance of the capacitor components. If you enter the From value and To value, all the capacitors between these values will come out.
5) Voltage Rating (V): The voltage rating value of the capacitor components. If you enter the From value and To value, all the capacitors between these values will come out. The default From value is about 10/9 times by the input voltage in order to remove the unwanted components.
6) Package: The material of the capacitor components. The package of 1206, 1210 and 1812 are available.
7) Quantity: The number of the output capacitor in parallel.
(2) The Ceramic Type Output Capacitor
When user clicks on the output capacitor C3, a capacitor database for searching will come out.

Here are some descriptions of the features on this page.
1) Value from Database: If this radio button is selected, the capacitor database section(3) will be enabled. User can select a capacitor from the given ceramic capacitor database and set its quantity.
2) NS: If this radio button is selected, it means that the capacitor is disconnected.
For others, the settings are similar to the input capacitor. Please refer to the description in The Input Capacitor C1 .
(3) The Electrolytic Type Output Capacitor
If user clicks the output capacitor C4, the dialog for edit will come out.

Here are some descriptions of the features on this page.
1) NS: If this radio button is selected, it means that the capacitor is disconnected.
2) Create a Custom Part: If this radio button is selected, the input boxes in Custom Part section(4) will be enabled. The capacitance and the ESR can be input directly.
3) Value from Database: If this radio button is selected, the capacitor database section(5) will be enabled. User can select a capacitor from the given electrolytic capacitor database and set its quantity.
(4) The Output Inductor L
If user clicks the output inductor L, the inductor database for searching will come out. Then, you can key the filter conditions to find the expected component.

The filter conditions include the following items:
1) Part Number: The part number of the inductor components.
2) Vendor: The vendor of the inductor components.
3) Package: The package of the inductor components.
4) Inductance (uH): The inductance of the inductor components. If user enters the From value and To value, all the inductors between these values will come out.
5) SatCurrent(A): The saturation current value of the inductor components. If user enters the From value and To value, all the inductors between these values will come out.
6) DCR (mOhm): The DC resistance value of the inductor components. If user enters the From value and To value, all the inductors between these values will come out.
(5) The Low Side Switch M1
If the selected chip is a synchronous part and its synchronous switch is outside the chip, the switch M1 can be edited.
If user clicks the switch M1 and goes into the MOSFET database, the MOSFET database for searching will come out. And user can key the filter conditions to find the expected component.

The filter conditions include the following items:
1) Part Number: The part number of the MOSFET components.
2) Vendor: The vendor of the MOSFET components.
3) Package: The package of the MOSFET components.
4) Voltage (V): The voltage rating value of the MOSFET components. If user enters the From value and To value, all the MOSFET whose voltage rating value between these values will come out.
5) Rds (mOhm): The on resistance value of the MOSFET components. If user enters the From value and To value, all the MOSFET whose on resistance value between these values will come out.
6) Qg (nC): The gate charge value of the MOSFET components. If user enters the From value and To value, all the MOSFET whose gate charge value between these values will come out.
(6) The Low Side Switch D1
If the selected chip is a non-synchronous part, the diode D1 can be edited.
If user clicks the switch D1 and goes into the diode database, the diode database for searching will come out. And user can key the filter conditions to find the expected component.

The filter conditions include the following items:
1) Part Number: The part number of the diode components.
2) Vendor: The vendor of the diode components.
3) Package: The package of the diode components.
4) VoltageVRRM (V): The voltage rating value of the diode components. If user enters the From value and To value, all the diode whose voltage rating value between these values will come out.
5) CurrentRating (A): The current rating value of the diode components. If user enters the From value and To value, all the diode whose current rating value between these values will come out.
6) Vdrop (V): The forward voltage drop value of the diode components. If user enters the From value and To value, all the diode whose forward voltage drop value between these values will come out.
5.2 Compensation Components Edit
The compensation components can be edited whenever needed. If user hovers the cursor around a compensation component, the cursor will turn into a palm symbol which means that the component is allowed to be changed. Left-click the component with mouse, the corresponding dialog box for editing will appear.
The compensation components which can be edited include components on the FB branch and components on the COMP pin. When user clicks on a resistor component, a resistance edit box will be shown.
The resistance can be input directly through the keyboard. Note: the unit is kOhm.

When user clicks on the compensation capacitor, a capacitor searching dialog will be shown.
1) Value from Database: It means that user want to choose the capacitor from this database if this radio button is selected.
2) NS: It means that the capacitor is disconnected and goes to Type 2 compensation networks if this radio button is selected.
3) Capacitance: Please input the capacitance range to search the capacitor.
4) Package: The package of the capacitor.

6. Recalculate
In general, user can follow the steps below to create a design using MPS DC/DC Designer.
Step1: Select target chip.
Step2: Set input specs and click on Recalculate button to get the recommend results.
Step3: Click on the editable component in the SCH area to modify it when needed, and then click on Recalculate button to do calculation.

In order to help user to use the MPS DC/DC Designer more easily, here are some things to be aware of.
6.1 Automatic Power Stage Components Calculation
The MPS DC/DC Designer can give user a power stage solution automatically according to the input parameters. However, this function only works when no power stage components are editted or the Manually Change Power Stage Components button is not checked.
If user wants to get the power stage components automatically, please input the main and optional parameters first, then makes sure the above conditions are meet, the final step is to click the Recalculate button at the bottom of the Design Target section.
6.2 Automatic Compensation Components Calculation
Compensation components will be automatically calculated in the following two cases.
1) Click the "Recalculate" button when no compensation parameters are modified.<
2) Click the Automatic Compensation button or Recalculate Compensation button when their are available.
Note: When any of the compensation components are edited, the Automatic Compensation button or Recalculate Compensation button will change from unavailable to available.
6.3 Manually Edit Power Stage Components
If user wants to change the power stage components by hand, the first thing is to make sure the Manually Change Power Stage Components button is checked, and then, user can click and change them freely. Please note that the unedited power stage components will keep their current values unchanged. It is useful to analyze the performance with user's specified power stage components.
6.4 Manually Edit Compensation Components
If user wants to change the compensation components by hand, user can click the corresponding component and change it directly at any time. Please note that the unedited compensation components will keep their current values unchanged. It is useful to analyze the small signal performance with user's specified compensation components.
7. Performance Analysis
The software MPS DC/DC Designer offers the user many system performance results that may include input and output AC ripple, efficiency and power loss, small signal bode plot, load transient result, typical waveform, layout guide information and so no. The following section will take you to go through the performance result in detail.
7.1 Calculated Specs. Results

Input Voltage Ripple (mV): The calculated result of the peak to peak input voltage AC ripple value.
Output Voltage Ripple (mV): The calculated result of the peak to peak output voltage AC ripple value.
Inductor Current Ripple (A): The calculated result of the peak to peak inductor current AC ripple value.
Calculated Bandwidth (kHz): The calculated result of the gain crossover frequency of the system small signal loop gain.
Phase Margin (degree): The calculated result of the phase value of the system small signal loop gain at the gain crossover frequency.
Gain Margin (dB): The negative value of the gain value of the system small signal loop gain at the phase crossover frequency.
Output Transient Voltage Ripple (mV): The calculated result of the peak to peak output voltage AC ripple value due to the load current transient change.
Efficiency (%): The calculated result of the efficiency value at the current system solution.
7.2 Typical Waveforms

For most parts, MPS DC/DC Designer will show user four key point waveforms in order to help user to know about the power system's operating performance.
1) Output Voltage Ripple Waveform: The output AC voltage ripple waveform. It is determined by the output inductor and the output capacitor with given input parameters.
2) Switching Waveform: The output AC voltage ripple waveform. It is determined by the output inductor and the output capacitor with given input parameters.
3) Input Voltage Ripple Waveform: The input AC voltage ripple waveform. It is determined by the output inductor and the input capacitor with given input parameters.
4) Inductor Current Waveform: The current flowing through the output inductor. It is determined by the inductance value with given input parameters.
7.3 Small Signal Bode Plot
For some parts, the small signal performance can be got easily with MPS DC/DC Designer. And with the software, the power stage model, compensation network model and the total loop gain which is equal to the power stage transfer function times by compensation network transfer function can be analyzed respectively. In order to get the result, user can switch the function button optionally. And for each figure, the gain and the phase are plotted respectively.

7.4 Load Transient Output Ripple
For some parts, MPS DC/DC Designer can give the simulation results of the output voltage ripple when the load current has the transient change. This is very useful for user to evaluate the system performance when the design sometimes has this special requirement. And the detailed result will be shown if user click the corresponding Transient Output Ripple button.

In the figure shown below, the upper waveform is the AC output voltage ripple due to the load change, the below one is the output current change waveform. In addition, the figure shows the transient condition and result below the waveforms.
1) High Current of Transient (A): The high value of the transient output current.
2) Low Current of Transient (A): The low value of the transient output current.
3) Transient Slew Rate (A/μs): The slew rate of the transient output current.
4) Maximum (mV): The peak voltage ripple value due to the high load change to the light load.
5) Minimum (mV): The peak voltage ripple value due to the light load change to the high load.
6) Peak-Peak (mV): The peak to peak voltage ripple value due to the load current transient change.
7.5 Efficiency and Power Loss Analysis
For most parts, MPS DC/DC Designer can offer the user the efficiency and power loss Waveform in order to help user to evaluate the power loss for the current power system.
The efficiency is calculated according to the formula below:

The power loss is calculated according the formula below:

Where,
Vo is the mean output voltage value,
Io is the mean output current value,
Vin is the mean input voltage value,
Iin is the mean output current value.
The detailed waveforms are shown in the figure below.

7.6 Bill of Materials
For each design, the software MPS DC/DC Designer can generate a BOM table which includes all the components used in the current design. The BOM table is shown below.
Export to XLS button offers user to save the BOM table as the xls type file.

7.7 Layout Information
As we know, the layout is very important in a power system design. So, MPS DC/DC Designer also has the layout information guide to the user. Here, user can find the recommended layout notices and the layout example which is very useful and important.
Gently note that this guide is a general one and may not be suitable for all situations!

8. Warning and Notice
8.1 Minimum On Time Limit Warning
If user inputs an improper parameter, the chip may not able to output the desired output voltage due to the minimum on time limit. It usually happens when user input a too large max.input voltage, or too small output voltage, or too high switching frequency. Then the following warning will appear. The warning notices user to input a lower input voltage or switching frequency.

8.2 Maximum On Time Limit Warning
If user inputs an improper parameter, the chip may not able to output the desired output voltage due to the maximum on time limit. It usually happens when user inputs a too small min. input voltage, or too large output voltage. Then the following warning will appear. The warning notices user to input a higher min. input voltage or lower output voltage.

8.3.Stability Warning
If user inputs some improper parameters, the chip may be unstable. Then the following warning will appear.

Here are some possible solutions.
1) Increase inductance.
2) Increase output capacitance if ceramic cap is selected.
3) Increase output capacitance and ESR value if electrolytic cap is selected.
4) Reduce compensation parameters. Such as reduce Rslope, Clsope, Cr, etc
5) Try other compensation type.
8.4.Out of Range Warning
8.4.1 Switching Frequency Warning
If user inputs an improper parameter, the chip may not able to output the desired output voltage due to the minimum off time limit. Then the following warning will appear.

Here are some possible solutions.
1) Increase the input voltage.
2) Lower the output voltage.
3) Lower the switching frequency.
4) Select the inductor Lout with lower DCR.
8.4.2 Slope Ripple Warning
If user inputs some improper parameters, the calculated external slope ripple will be out of range. Then the following warning will appear.

Here are some possible solutions.
1) Increase inductance.
2) Increase output capacitance if ceramic cap is selected.
3) Increase output capacitance and ESR value if electrolytic cap is selected.
4) Increase Rslope or Cslope.
If user inputs some improper parameters, the calculated slope ripple will be out of range. Then the following warning will appear.

Here are some possible solutions.
1) Increase inductance.
2) Increase output capacitance if ceramic cap is selected.
3) Increase output capacitance and ESR value if electrolytic cap is selected.
4) Increase Cr.
8.4.3 Cslope Warning
If user inputs an improper Cslope value, the following warning will appear. The warning notices user to select a capacitor that the capacitance between the two given values.

8.4.4 Cr Warning
If user inputs an improper Cr value, the following warning will appear. The warning notices user to select a capacitor that the capacitance between the two given values.

8.4.5 RFB1 Warning
If user inputs some improper parameters, the chip may not able to output the desired output voltage and the calculated RFB1 will be unreasonable. Then the following warning will appear.

Here are some possible solutions.
1) Increase inductance.
2) Increase output capacitance if ceramic cap is selected.
3) Increase output capacitance if electrolytic cap is selected.
4) Increase output voltage or switching frequency.
5) Adjust RFB2.
6) Try other compensation type.
9. Support
For other information please visit the following address.
http://www.monolithicpower.com
http://www.monolithicpower.com/Design-Support/DC-DC-Designer-online